MC_MoveAbsolute (FB)
FUNCTION_BLOCK MC_MoveAbsolute
This function block commands a controlled motion to a specified absolute position.
This action completes with velocity zero if no further action are pending.
If there is only one mathematical solution to reach the commanded position (like in linear systems), the value of the input direction is ignored.
For modulo axis, valid absolute position values are in the range of [0, [360, (360 is excluded), or corresponding range. The application, however, may shift the commanded position of MC_MoveAbsolute into the corresponding modulo range. For relative positions, modulo 360 is applicable.
The Enum type “shortest_way” is focused to a trajectory which will go through the shortest route. The decision which direction to go is based on the current position where the command is issued.
Note
With every rising edge at “Execute”, modified input parameters will be used.
- Example
The following figure shows two examples of the combination of two function blocks MC_MoveAbsolute.
1. The left part of timing diagram illustrates the case if the second function block is called after the first one. If first reaches the commanded position of 6000 (and the velocity is 0) then the output Done causes the second function block to move to the position 10000.
2. The right part of the timing diagram illustrates the case if the second move function block starts the execution while the first function block is still executing. In this case the first motion is interrupted and aborted by the test signal during the constant velocity of the first Function Block. The second function block moves directly to the position 10000 although the position of 6000 is not yet reached
Note
Input validation is done at the rising edge of Execute. If function block is in Active/Busy state, new value at input will not be validated. If value passed is invalid function block will continue execution with paraMaxVelocityAppl value i.e., (Max application velocity).
- InOut:
Scope
Name
Type
Comment
Input
ExecuteBOOLStarts the function block at rising edge
PositionLREAL[u] Reference position. Range: Maximum range is 16#7FFFFFFF in increments, if configured in units, range will be limited to equivalent of 16#7FFFFFFF increments
VelocityLREAL[u/s] Value of the maximum velocity (not necessarily reached). Range: >0. If value = 0, velocity will be equal to the parameter paraMaxVelocityAppl
AccelerationLREAL[u/s°°2] Value of the acceleration (increasing energy of the motor). Range: >0. If value = 0, Acceleration will be equal to parameter paraMaxAccelerationAppl.If value > 0 and <= 1,Acceleration will be limited to 1.
DecelerationLREAL[u/s°°2] Value of the deceleration (decreasing energy of the motor). Range: >0. If value = 0, Deceleration will be equal to parameter paraMaxDecelerationAppl.If value > 0 and <= 1,Deceleration will be limited to 1.
JerkLREAL[u/s°°3] Value of the Jerk. Range: >=0
DirectionPositive, shortest, negative, current, positive_stop, negative_stop, Current_Stop
BufferModeNot supported, default mcABORTING used
Output
DoneBOOLShows the status of the function block. Done = TRUE if the execution is finished
BusyBOOLThe function block is not finished
ActiveBOOLIndicates that the function block has control on the axis
CommandAbortedBOOLCommand is aborted by another command from other PLCopen function block
ErrorBOOLSignals that error has occurred within function block
ErrorIDError identification. For error details refer to Enumeration ERROR_ID
Inout
AxisReference to axis