MC_HaltSuperImposed (FB)

FUNCTION_BLOCK MC_HaltSuperImposed

This function block commands a halt to all superimposed motions of the axis. The underlying motion is not interrupted.

../../../../../../_images/plcopen.png
InOut:

Scope

Name

Type

Comment

Input

Execute

BOOL

Starts the function block at rising edge

Deceleration

LREAL

[u/s°°2] Value of the deceleration (decreasing energy of the motor). Range: >0. If value = 0, Deceleration will be equal to parameter paraMaxDecelerationAppl.If value > 0 and <= 1,Deceleration will be limited to 1.

Jerk

LREAL

[u/s°°°3] Value of the jerk. Range: >=0

BufferMode

MC_BufferMode

Not supported, default mcABORTING used

Output

Done

BOOL

Shows the status of the function block. Done = TRUE if the execution is finished

Busy

BOOL

The function block is not finished and new output values are to be expected

Active

BOOL

Indicates that the function block has control on the axis

CommandAborted

BOOL

Command is aborted by another command from other PLCopen function block

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

Inout

Axis

Axis_Ref

Reference to axis