MotionControlExtension (LIB)
- Version
1.0.0.41
- Namespace
AC500_MotionControlExtension
- Author
None
- Placeholder
AC500_MotionControlExtension
Description 1
This library is an extension of the PS5611 Motion Control library and the Ecat_CiA402 library.
This library contains ABB Specific (MCA) and Central Motion control (CMC) function blocks. Using these function blocks one can realize the Motion control functionalities such as: XYGroup interpolation, Quict stop the drive, Driving motor in PV, PT, CST mode, Enhanced homing, Enhanced Cam related operation and so on.
This Library needs PLC based runtime license for using the features.
Copyright: We reserve all rights in these programs and the information therein. Reproduction, use or disclosure to third parties without express authority is strictly forbidden. (c) 2006-2024 ABB, all rights reserved
Contents:
01_PLCopenABB SpecificCam ExtensionEtherCATMCA_DriveCheckReadyToEnable(FB)MCA_DriveEnableImmediateApply(FB)MCA_DriveParametersSave(FB)MCA_DriveSetOperatingMode(FB)MCA_GetABBServoErrorDescription(FB)MCA_MoveFeed(FB)MCA_MoveVelocity_PV(FB)MCA_QuickStop(FB)MCA_TorqueControl_CSTOL(FB)MCA_TorqueControl_PT(FB)MCA_TorqueProfile_CSTOL(FB)MCA_TouchProbeECAT(FB)MCA_TouchProbeECATFiltering(FB)
GenericHomingMCA MultiAxisXYGroup
03_DeviceInterfaceData typesFunctionsGlobalConstantsGlobalTextList(Text List)ImagePool(Image Pool)Visualizationshistory(STRUCT)
Indices and tables
- 1
- Based on ABB_MotionControlExtension_AC500.library, last modified 22.10.2025, 11:56:03. LibDoc 4.6.0.0-r.29The content file ABB_MotionControlExtension_AC500.json was generated with Automation Builder 2.9 on 22.10.2025, 11:57:15.