ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
Enumeration of the Error ID, describes the details of each error generated by function blocks.
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
16#0
1: No Error
INVALID_INPUT1
16#4010
2: Invalid value at input 1
INVALID_INPUT2
16#4020
3: Invalid value at input 2
LOW_INPUT2
16#4021
4: Low value at input 2
WRONG_PARAMETER_2_3
16#4023
5: Value at input 3 is greater than value at input 2
WRONG_PARAMETER_3_4
16#4034
6: Value at input 4 is greater than value at input 3
WRONG_PARAMETER_4_5
16#4045
7: Value at input 5 is greater than value at input 4
INVALID_INPUT3
16#4030
8: Invalid value at input 3
INVALID_INPUT4
16#4040
9: Invalid value at input 4
INVALID_INPUT5
16#4050
10: Invalid value at input 5
LOW_INPUT5
16#4051
11: Low value at input 5
INVALID_INPUT6
16#4060
12: Invalid value at input 6
LOW_INPUT6
16#4061
13: Low value at input 5
INVALID_INPUT7
16#4070
14: Invalid value at input 7
LOW_INPUT7
16#4071
15: Low value at input 7
LOW_INPUT9
16#4091
16: Invalid value at input 9
INVALID_INPUT9
16#4090
17: Invalid value at input 9
INVALID_INPUT10
16#40A0
18: Invalid value at input 10
INVALID_INPUT11
16#40B0
19: Invalid value at input 11
INVALID_INPUT12
16#40C0
20: Invalid value at input 12
LOW_INPUT14
16#40E1
21: Invalid value at input 14
LOW_INPUT15
16#40F1
22: Low value at input 15
HIGH_INPUT15
16#40F2
22: Low value at input 15
TUNE_FAULT
16#7280
23: Tune fault is generated - bit 0 of wErrors of TectProcessStatusType
TC_FAULT1
16#7281
24: TC_Fault1 is generated when Actual Temperature is less than tsMachineSet.rTcMin or greater than tsMachineSet.rTcMax - bit 1 of wErrors of TectProcessStatusType
TC_FAULT2
16#7282
25: TC_Fault2 is generated when tsMachineSet.uiMinTempChange is not achieved within tsMachineSet.uiChangeTime - Bit 2 of wErrors of TectProcessStatusType
HIGH_HIGH_TEMP_FAULT
16#7283
26: When the High High Temperature Fault is generated - Bit 3 of wErrors of TectProcessStatusType. Actual temperature is greater than the high high Temperature.
LOW_LOW_TEMP_FAULT
16#7284
27: When the Low Low Temperature Fault is generated - Bit 4 of wErrors of TectProcessStatusType.Actual temperature is lower than the low low Temperature.
WRONG_TEMP_LIMITS
16#7291
28: When the configured limits is not in the order of TectMachineSet.TcMax > TectMachineSet.rHighHighTemp > TectProcessSet.rHighTemp > TectProcessSet.rLowTemp > TectMachineSet.rLowLowTemp- Bit 12 of wErrors of TectProcessStatusType + Note: Two Temperature Limits must also not be equal
CAA_FILE_ERROR
16#7296
29: CAA file Error, Please refer Status output for more details.
GROUP_FB_CALLING_ERROR
16#7297
30: No group function block call possible - internal group function call for TectTempControl or TectPwm8 failed
TIMEOUT
16#7298
31: Timeout of one operation State
READ_DATA_FAILED
16#7299
32: Read data failed: No correct format of data items
ALL_ZONES_NOT_READ
16#729B
33: Less zone data availabe in CSV recipe file than requested from TectRecipe function block
ASSIGNMENT_WRONG
16#729C
34: Zone size and zone index are not assigned as byGroupSize = 0 in the structure
NO_OF_ZONES_WRONG_CONFIG
16#729D
35: Number of zones configured is more than the actual number of zones
LOGGING_NOT_COMPLETE
16#729A
36: Restart of the Enable is required since last log saving is not complete