MotionControlEco (LIB)

Version

1.1.0.9

Namespace

AC500_MotionControlEco

Author

Placeholder

AC500_MotionControlEco

Description 1

The library provides function blocks to use the PWM and PTO of the eCoV3 PLC to realize the motion control applications.

Along with the kernel function blocks in this library user can use the MC, MCA function blocks from the AC500_MotionControl Library to realize various motion control functionalities like camming, homing and so on. For more details of the available function blocks refer to ABB_MotionControl_AC500 library.

Refer the Automation Builder online help for details on the eCoV3 PLC configuration of PWM, PTO and other limitations.

Copyright: We reserve all rights in these programs and the information therein. Reproduction, use or disclosure to third parties without express authority is strictly forbidden. (c) 2006-2021 ABB, all rights reserved

Contents:

Indices and tables

1
Based on ABB_MotionControlEco_AC500.library, last modified 06.11.2024, 15:34:12. LibDoc 4.6.0.0-r.29
The content file ABB_MotionControlEco_AC500.json was generated with Automation Builder 2.8 on 06.11.2024, 15:34:23.