MC_WriteParameter (FB)
FUNCTION_BLOCK MC_WriteParameter
It will support the Parameters defined as “standard” in the PLCopen. These parameters will be transfered to the units as used for PLCopen function blocks
When a drive based axis implementation is used, the function block writes the value of a drive specific parameter or a PLCopen parameter. When the Central Motion Control axis implementation is used, a parameter according to the list PLCopen parameter is written
Parameter No(PN) |
Name |
DataType |
Min. |
Max. |
Default |
R/W |
Comments |
|---|---|---|---|---|---|---|---|
1 |
CommandedPosition |
DINT |
R |
Commanded Position |
|||
2 |
SWLimitPos |
DINT |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Positive Software limit switch position |
3 |
SWLimitNeg |
DINT |
-2147483647 |
2147483647 |
-2147483647 |
R/W |
Negative Software limit switch position |
4 |
EnableLimitPos |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable positive software limit switch |
5 |
EnableLimitNeg |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable negative software limit switch |
6 |
EnablePostLagMonitoring |
BOOL |
FALSE |
TRUE |
TRUE |
R/W |
Enable monitoring of position lag (following error) |
7 |
MaxPositionLag |
DINT |
1 |
2147483647*** |
R |
Maximal position lag |
|
8 |
MaxVelocitySystem |
DINT |
32767 |
R |
Maximal allowed velocity of the axis in the motion system |
||
9 |
MaxVelocityAppl |
DINT |
0** |
32767 |
32767 |
R/W |
Maximal allowed velocity of the axis in the application |
10 |
ActualVelocity |
DINT |
-32767 |
32767 |
R |
Actual velocity |
|
11 |
CommandedVelocity |
DINT |
-32767 |
32767 |
R |
Commanded Velocity |
|
12 |
MaxAccelerationSystem |
DINT |
32767 |
R |
Maximal allowed acceleration of the axis in the motion system |
||
13 |
MaxAccelerationAppl |
DINT |
10 |
32767 |
32767 |
R/W |
Maximal allowed acceleration of the axis in the application |
14 |
MaxDecelerationSystem |
DINT |
32767 |
R |
Maximal allowed deceleration of the axis |
||
15 |
MaxDecelerationAppl |
DINT |
10 |
32767 |
32767 |
R/W |
Maximal allowed deceleration of the axis |
16 |
MaxJerk |
DINT |
0* |
2147483647 |
2147483647 |
R/W |
Maximal allowed jerk of the axis |
2001 |
MODULO_NOMINATOR |
DINT |
1 |
2147483647 |
1 |
R/W |
ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE |
2002 |
MODULO_DENOMINATOR |
DINT |
1 |
2147483647 |
1 |
R/W |
ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE |
2003 |
EnableLimit2Decelerate |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable software limit switches to decelerate |
2004 |
EnableLimitAbort |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable that software limit switches will abort ongoing movement |
2005 |
EnableLimitVelocity |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
If the velocity is limited the unmoved position will be covered whenever possible |
2006 |
SWLimit2DecPos |
LREAL |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Used as end position for EnableLimit2Decelerate |
2007 |
SWLimit2DecNeg |
LREAL |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Used as end position for EnableLimit2Decelerate |
2008 |
MaxPositionGapLL |
LREAL |
0 |
214748364700 |
0 |
R/W |
Used to stop the ongoing movement if position is behind |
*0 means: no limitation of jerk is performed.
**Axis will stay in stop.
***Is modified by CMC_Axis_Control_Parameter, the maximum Value is calculated in increments, the value which is delivered by ReadParameter will be given in [u].
- InOut:
Scope
Name
Type
Comment
Input
ExecuteBOOLStarts the function block at rising edge
ParameterNumberWORDNumber of the parameter (correspondence between number and parameter is to be specified later)
ValueDINTNew value of the specified parameter
Output
DoneBOOLShows the status of the function block. Done = TRUE if the execution is finished
BusyBOOLThe function block is not finished
ErrorBOOLSignals that error has occurred within function block
ErrorIDError identification. For error details refer to Enumeration ERROR_ID
Inout
AxisReference to axis