MC_WriteBoolParameter (FB)

FUNCTION_BLOCK MC_WriteBoolParameter

It will support the Parameters defined as “standard” in the PLCopen. These parameters will be transfered to the units as used for PLCopen function blocks

../../../../../../_images/plcopen.png

When a drive based axis implementation is used, the Function Block writes the value of a drive specific BOOL parameter or a PLCopen BOOL parameter. When the Central Motion Control axis implementation is used, a BOOL parameter according to the list PLCopen parameter is written

Parameter No(PN)

Name

DataType

Min.

Max.

Default

R/W

Comments

1

CommandedPosition

DINT

R

Commanded Position

2

SWLimitPos

DINT

-2147483647

2147483647

2147483647

R/W

Positive Software limit switch position

3

SWLimitNeg

DINT

-2147483647

2147483647

-2147483647

R/W

Negative Software limit switch position

4

EnableLimitPos

BOOL

FALSE

TRUE

FALSE

R/W

Enable positive software limit switch

5

EnableLimitNeg

BOOL

FALSE

TRUE

FALSE

R/W

Enable negative software limit switch

6

EnablePostLagMonitoring

BOOL

FALSE

TRUE

TRUE

R/W

Enable monitoring of position lag (following error)

7

MaxPositionLag

DINT

1

2147483647***

R

Maximal position lag

8

MaxVelocitySystem

DINT

32767

R

Maximal allowed velocity of the axis in the motion system

9

MaxVelocityAppl

DINT

0**

32767

32767

R/W

Maximal allowed velocity of the axis in the application

10

ActualVelocity

DINT

-32767

32767

R

Actual velocity

11

CommandedVelocity

DINT

-32767

32767

R

Commanded Velocity

12

MaxAccelerationSystem

DINT

32767

R

Maximal allowed acceleration of the axis in the motion system

13

MaxAccelerationAppl

DINT

10

32767

32767

R/W

Maximal allowed acceleration of the axis in the application

14

MaxDecelerationSystem

DINT

32767

R

Maximal allowed deceleration of the axis

15

MaxDecelerationAppl

DINT

10

32767

32767

R/W

Maximal allowed deceleration of the axis

16

MaxJerk

DINT

0*

2147483647

2147483647

R/W

Maximal allowed jerk of the axis

2001

MODULO_NOMINATOR

DINT

1

2147483647

1

R/W

ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE

2002

MODULO_DENOMINATOR

DINT

1

2147483647

1

R/W

ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE

2003

EnableLimit2Decelerate

BOOL

FALSE

TRUE

FALSE

R/W

Enable software limit switches to decelerate

2004

EnableLimitAbort

BOOL

FALSE

TRUE

FALSE

R/W

Enable that software limit switches will abort ongoing movement

2005

EnableLimitVelocity

BOOL

FALSE

TRUE

FALSE

R/W

If the velocity is limited the unmoved position will be covered whenever possible

2006

SWLimit2DecPos

LREAL

-2147483647

2147483647

2147483647

R/W

Used as end position for EnableLimit2Decelerate

2007

SWLimit2DecNeg

LREAL

-2147483647

2147483647

2147483647

R/W

Used as end position for EnableLimit2Decelerate

2008

MaxPositionGapLL

LREAL

0

214748364700

0

R/W

Used to stop the ongoing movement if position is behind

*0 means: no limitation of jerk is performed.

**Axis will stay in stop.

***Is modified by CMC_Axis_Control_Parameter, the maximum Value is calculated in increments, the value which is delivered by ReadParameter will be given in [u].

InOut:

Scope

Name

Type

Comment

Input

Execute

BOOL

Starts the function block at rising edge

ParameterNumber

WORD

Number of the parameter (correspondence between number and parameter is to be specified later)

Value

BOOL

New value of the specified parameter

Output

Done

BOOL

Shows the status of the function block. Done = TRUE if the execution is finished

Busy

BOOL

The function block is not finished

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

Inout

Axis

Axis_Ref

Reference to axis