MC_ReadActualPosition (FB)
FUNCTION_BLOCK MC_ReadActualPosition
This function block returns the actual position.
- InOut:
Scope
Name
Type
Comment
Input
EnableBOOLRead continuously on “TRUE”
ValueSourceDefault: MCActualValue: Decide to use the actual position or reference position of axis
Output
ValidBOOLValue is available
ErrorBOOLSignals that error has occurred within function block
ErrorIDError identification. For error details refer to Enumeration ERROR_ID
PositionLREAL[u] New absolute position
Inout
AxisReference to axis