SysComSettingsEx (STRUCT)
TYPE SysComSettingsEx : STRUCT
<category>Com port extended settings</category> <description>: This structure can be used to get and set the settings of a COM port.
NOTE: The difference of this structure to SysComSettingsEx2 are the 2 members bDtrControl and bRtsControl! Here you can specify only BOOL instead of BYTE values in SysComSettingsEx2!
</description>
- InOut:
Name
Type
Comment
byByteSizeBYTE<element name=”byByteSize” TYPE=”IN”>Number of bits/BYTE, 4-8</element>
bBinaryBOOL<element name=”bBinary” TYPE=”IN”>Binary mode, no EOF check</element>
bOutxCtsFlowBOOL<element name=”bOutxCtsFlow” TYPE=”IN”>CTS handshaking on output</element>
bOutxDsrFlowBOOL<element name=”bOutxDsrFlow” TYPE=”IN”>DSR handshaking on output</element>
bDtrControlBOOL<element name=”bDtrControl” TYPE=”IN”>DTR flow control</element>
bDsrSensitivityBOOL<element name=”bDsrSensitivity” TYPE=”IN”>DSR Sensitivity</element>
bRtsControlBOOL<element name=”bRtsControl” TYPE=”IN”>Rts flow control</element>
bTXContinueOnXoffBOOL<element name=”bTXContinueOnXoff” TYPE=”IN”>XOFF continues Tx</element>
bOutXBOOL<element name=”bOutX” TYPE=”IN”>XON/XOFF out flow control</element>
bInXBOOL<element name=”bInX” TYPE=”IN”>XON/XOFF in flow control</element>
byXonCharBYTE<element name=”XonChar” TYPE=”IN”>Tx AND Rx XON character</element>
byXoffCharBYTE<element name=”XoffChar” TYPE=”IN”>Tx AND Rx XOFF character</element>
wXonLimWORD<element name=”XonLim” TYPE=”IN”>transmit XON threshold</element>
wXoffLimWORD<element name=”XoffLim” TYPE=”IN”>transmit XOFF threshold</element>