SysComSetTimeout (FUN)
FUNCTION SysComSetTimeout : RTS_IEC_RESULT
- <description>Set the timeout of the specified serial interface (hardware timeout).
The Timeout is the time between two received or sent characters until the read or write operation will return. Typically this value should be 0 (returns immediately)</description>
<result><p>RESULT: Returns the runtime system error code (see CmpErrors.library).</p></result>
- InOut:
Scope
Name
Type
Comment
Return
SysComSetTimeoutRTS_IEC_RESULTInput
hComRTS_IEC_HANDLE<param name=”hCom” type=”IN”>Handle to com port</param>
ulTimeout<param name=”ulTimeout” type=”IN”>Timeout in milliseconds for the read and write operation to set</param>