SysComSetSettings (FUN)
FUNCTION SysComSetSettings : RTS_IEC_RESULT
<description>Set the parameter of the interface specified by handle. Use SysComSetSettings2()! This function should only be used for backward compatibility! </description> <result><p>RESULT: Returns the runtime system error code (see CmpErrors.library).</p></result>
- InOut:
Scope
Name
Type
Comment
Return
SysComSetSettingsRTS_IEC_RESULTInput
hComRTS_IEC_HANDLE<param name=”hCom” type=”IN”>Handle to com port</param>
pSettingsPOINTER TO SysComSettings
<param name=”pSettings” type=”IN”>Pointer to new settings</param>
pSettingsExPOINTER TO SysComSettingsEx
<param name=”pSettingsEx” type=”IN”>OPTIONAL: Pointer to extended settings or 0</param>