CmpEventMgr Interfaces (LIB)
- Version
3.5.17.0
- Author
CODESYS Development GmbH
Description 1
This library provides access to the event manager of the runtime system. The event manager handles events from components (provider) and transmits these events via callbacks to IEC consumers (functions or function-blocks).
Contents:
Indices and tables
- 1
- Based on CmpEventMgr_Itfs.library, last modified 20.04.2021, 15:40:36. LibDoc 4.6.0.0-r.29The content file CmpEventMgr_Itfs.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 15:40:36.