CmpOPCUAProviderAlarmConfiguration Implementation (LIB)

Version

3.5.21.0

Author

CODESYS Development GmbH

Placeholder

CmpOPCUAProviderAlarmConfiguration Implementation

Description 1

This library provides the external runtime interface for sending alarms from the CODESYS Alarm Configuration to the CODESYS OPC UA server. This API is not intended to be used directly by an application. Use the CompatibleAlarmManagerToOpcUaServer library to connect alarms when using the symbol configuration. Configure the mapping between AlarmGroup and Symbol Set if you are using the CODESYS Communication Manager.

Indices and tables

1
Based on CmpOPCUAProviderAlarmConfiguration Implementation.library, last modified 10.03.2025, 15:48:31. LibDoc 4.6.0.0-r.29
The content file CmpOPCUAProviderAlarmConfiguration Implementation.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 10.03.2025, 15:48:35.