CmpTls (LIB)
- Version
3.5.17.0
- Author
3S - Smart Software Solutions GmbH
- Placeholder
CmpTls
Description 1
Library, to manage TLS settings used by different other libraries.
- Use case:
With this library it is possible to create a desired TLS context and set thins up for different use cases.
With this library it is possible to establish TLS connection on static buffers. The content of the buffers have to be exchanged by the user of this library. If TCP should be used use SysSocket2 instead. This library offers a socket like interface of the TLS protocol.
Indices and tables
- 1
- Based on CmpTls.library, last modified 20.04.2021, 15:56:50. LibDoc 4.6.0.0-r.29The content file CmpTls.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 15:56:50.