IOL_PortStatusList (STRUCT)
TYPE IOL_PortStatusList : STRUCT
IO-Link PortStatusList
- InOut:
Name
Type
Comment
PortStatusInfoStatus information of the Port
PortQualityInfoStatus information on Process Data
RevisionIDBYTESDCI protocol revision of the Device
TransmissionRateEffective port transmission rate
MasterCycleTimeBYTEMaster cycle time
InputDataLengthBYTEInput data length as number of octets
OutputDataLengthBYTEOutput data length as number of octets
VendorIDUINTVendorID
DeviceIDUDINTDeviceID
NumberOfDiagsBYTEThe number of diagnosis entries stored in field DiagEntries
DiagEntriesARRAY [0..(IOL_Constants.MAX_PortStatus_DiagEntry - 1)] OF UDINT
Diagnosis entries. See IOL_GetEvent_UDINT