IOL_PortStatusInfo (ENUM)
TYPE IOL_PortStatusInfo :
Status information of the Port
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_DEVICE
0
No communication (COMLOST). How-ever, Port configuration IOL_MANUAL or IOL_AUTOSTART was set (see Table E.3).
DEACTIVATED
1
Port configuration DEACTIVATED was set (see Table E.3).
PORT_DIAG
2
This value to be set If a DiagEntry indicates an upcoming diagnosis of the Port during startup, validation, and Data Storage (group error). Device is in PREOPERATE and DiagEntry contains the diagnosis cause.
PREOPERATE
3
This is only an intermediate state leading to OPERATE or PORT_DIAG.
OPERATE
4
This value to be set if the Device is in OPERATE, even in case of Device error.
DI_CQ
5
Port configuration “DI” was set (see Table E.3).
DO_CQ
6
Port configuration “DO” was set (see Table E.3).
PORT_POWER_OFF
254
SMI_PortPowerOffOn (see 11.2.14) caused the communication system to stop. All indications become obsolete according to the state machine in Figure 101 and shall be reported according to state transition Table 126.
NOT_AVAILABLE
255
PortStatusInfo currently not available