IOL_MasterIdent (STRUCT)
TYPE IOL_MasterIdent : STRUCT
Master Ident-data and basic capabilities of Master its Ports
- InOut:
Name
Type
Comment
VendorIDUINTUnique VendorID of the Master
DeviceIDUDINT4 octets long vendor specific unique identification of the Master
MasterTypeTyoe of Master
Features_1Supported features of this Master
MaxNumberOfPortsBYTEMaximum number (n) of ports of this Master
PortTypesARRAY [0..(IOL_Constants.MAX_MasterIdent_PortTypes - 1)] OF IOL_PortType
Array indicating for all n ports the type of port