MCA_PhasingReset (FB)

FUNCTION_BLOCK MCA_PhasingReset

This function block will reset any existing phasing for the axis.

It can just be called while the axis is in standstill.

../../../../../../_images/plcopen.png
InOut:

Scope

Name

Type

Comment

Input

Execute

BOOL

Starts the function block at rising edge

Output

Done

BOOL

Shows the status of the function block. Done = TRUE if the execution is finished

Busy

BOOL

The function block is not finished

Active

BOOL

Indicates that the function block has control on the axis

CommandAborted

BOOL

Command is aborted by another command from other PLCopen function block

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

AbsolutePhaseShift

LREAL

[u] Actual phase shift of master axis to slave axis, valid while function block is busy

Inout

Axis

Axis_Ref

Reference to axis