MCA_CamInfo (FB)
FUNCTION_BLOCK MCA_CamInfo
This function block gives an information which index is actually processed by the respective cam table.
- Precondition
Correct information is shown if the referenced cam table is still active.
The block will not check if the cam table is still active.
Note
User can utilize CAM editor in Automation builder to generate Cam table (MC_PProfile) automatically. For more details refer to Automation builder help.
- InOut:
Scope
Name
Type
Comment
Input
EnableBOOLActivate the function block
Inout
CamTableIDPrepared by MC_CamTableSelect and used with MC_CamIn or MCA_CamInDirect
Output
ActiveIndexINTActive Index, value always starts from zero, even if the CAM table array is started with a different value