MCA_Parameter (FB)
FUNCTION_BLOCK MCA_Parameter
This function block can be used to change the default values of the following parameters:
Target position window. The default value is 10 units.
Target velocity window. The default vaule is 10 units.
Maximum fieldbus delay. If this value will be exceeded then it will be assumed that there is a communication error
Note
The block MCA_Parameter has to be used to adjust the velocity limit when velocities < 10 u/s should be used (10 u/s: default value).
The parameter v_Window defines the limit for the axis to reach its target velocity or standstill
This detection will not work properly when smaller velocities are used, especially the block MC_StepLimitSwitch will not stop the axis when reaching the switch!
- InOut:
Scope
Name
Type
Initial
Comment
Input
BusDelayTIMETIME#1s0ms
A delay time to wait for fieldbus data. When the delay time is too long, the reaction time of function blocks might be increased, while when it is too short an error might be indicated although everything is ok
PosWindowLREAL10
The limit for the axis to reach it´s target position
V_WindowLREAL10
The limit for the axis to reach it´s target velocity
Inout
AxisReference to axis