MachineryDriveInterface (LIB)
- Version
1.0.0.2
- Namespace
AC500_MachineryDriveInterface
- Author
- Placeholder
AC500_MachineryDriveInterface
Description 1
To make the use of the E530 and ACS drive control over Modbus easier for the user, ABB has created a library of function blocks which offer an easy method to issue motion commands to the drive from the PLC.
Copyright:We reserve all rights in these programs and the information therein. Reproduction, use or disclosure to third parties without express authority is strictly forbidden. (c) 2006-2026 ABB, all rights reserved
Contents:
Indices and tables
- 1
- Based on ABB_MachineryDriveInterface_AC500.library, last modified 12.06.2026, 07:45:17. LibDoc 4.6.0.0-r.29The content file ABB_MachineryDriveInterface_AC500.json was generated with Automation Builder 2.9 on 12.06.2026, 07:46:20.