MDI_ReadPosition (FB)
FUNCTION_BLOCK MDI_ReadPosition
This function block makes the actual position available from the axis reference structure.
- InOut:
Scope
Name
Type
Initial
Comment
Input
EnableBOOLFALSE
Enable the function block.
Inout
AxisReference to the axis structure.
Output
ValidBOOLCompleted sourcing of valid data without error.
ErrorBOOLSignals that an error has occurred within function block.
ErrorIDContains the error code when there is an error.
ActualPositionREALActual position in user units, only for E530.