MDI_Reset (FB)
FUNCTION_BLOCK MDI_Reset
This function block is used to reset any axis error that is present.
- InOut:
Scope
Name
Type
Initial
Comment
Input
ExecuteBOOLFALSE
Starts the fault reset on a rising edge.
Inout
AxisReference to the axis structure.
Output
DoneBOOLSets to true when the axis no longer has an error present.
BusyBOOLSets to true while the function block is in progress.
ErrorBOOLSignals that an error has occurred within function block.
ErrorIDContains the error code when there is an error.