SysMCGetProcessBinding (FUN)
FUNCTION SysMCGetProcessBinding : RTS_IEC_RESULT
Function to read the binding of a process to core(s). .. note:: To obtain the binding of the current process hProcess may be RTS_INVALID_HANDLE. .. note:: To obtain the CoreIds set in CpuCoreBindingDesc use SysMCBDGetFirstID and SysMCBDGetNextID.
- InOut:
Scope
Name
Type
Comment
Return
SysMCGetProcessBindingRTS_IEC_RESULT- Returns the result.
ERR_OK: Call was successful.
ERR_PARAMETER: Parameter is invalid.
ERR_FAILED: Function failed for any reason on OS level.
ERR_NOTIMPLEMENTED: Function is not implemented.
ERR_NOT_SUPPORTED: Function is not supported.
Input
hProcessRTS_IEC_HANDLEHandle of the process or RTS_INVALID_HANDLE for current process.
pBindingDescPOINTER TO CpuCoreBindingDesc
Pointer to the binding description for the core binding.