SysMCGetNumOfCores (FUN)
FUNCTION SysMCGetNumOfCores : DWORD
Function to get the number of cores available for use by the runtime system.
- InOut:
Scope
Name
Type
Comment
Return
SysMCGetNumOfCoresDWORDReturns the number of cores.
Input
pResultPOINTER TO RTS_IEC_RESULT
- Pointer to a variable to return an error code (optional)
ERR_OK: Call was successful.
ERR_FAILED: Function failed for any reason on OS level.
ERR_NOTIMPLEMENTED: Function is not implemented.