CIFX_SYSTEM_CHANNEL_INFO (STRUCT)

TYPE CIFX_SYSTEM_CHANNEL_INFO : STRUCT

InOut:

Name

Type

Comment

bChannelType

USINT

!< 0x00 TYPE OF THIS channel

bReserved

USINT

!< 0x01 reserved

bSizePositionOfHandshake

USINT

!< 0x02 Size AND position OF the handshake cells

bNumberOfBlocks

USINT

!< 0x03 Number OF blocks in THIS channel

ulSizeOfChannel

UDINT

!< 0x04 Size OF channel in bytes

usSizeOfMailbox

UINT

!< 0x08 Size OF the send AND receive mailbox

usMailboxStartOffset

UINT

!< 0x0A Start offset OF the mailbox structure (see NETX_MAILBOX)

abReserved

ARRAY [0..3] OF BYTE

!< 0x0C:0x0F Reserved area