CIFX_COMMUNOICATION_CHANNEL_INFO (STRUCT)

TYPE CIFX_COMMUNOICATION_CHANNEL_INFO : STRUCT

InOut:

Name

Type

Comment

bChannelType

USINT

!< 0x00 TYPE OF THIS channel

bChannelId

USINT

!< 0x01 Channel / Port ID

bSizePositionOfHandshake

USINT

!< 0x02 Size and position of the handshake cells

bNumberOfBlocks

USINT

!< 0x03 Number of blocks in this channel

ulSizeOfChannel

UDINT

!< 0x04 Size of channel in bytes

usCommunicationClass

UINT

!< 0x08 Communication Class (Master, Slave…)

usProtocolClass

UINT

!< 0x0A Protocol Class (PROFIBUS, PROFINET….)

usProtocolConformanceClass

UINT

!< 0x0C Protocol Conformance Class (DPV1, DPV2…)

abReserved

ARRAY [0..1] OF BYTE

!< 0x0E:0x0F Reserved area