_FdDriverOpenP (FUN)

FUNCTION _FdDriverOpenP : CAA.HANDLE

Unmanaged implementation of FdDriverOpenP

InOut:

Scope

Name

Type

Comment

Return

_FdDriverOpenP

CAA.HANDLE

Input

usiNetId

USINT

number of FD-capable CAN interface [0..n]

uiNominalBaudrate

UINT

Baud rate used for arbitration. Unit: kBit/s

uiDataBaudrate

UINT

Baud rate used for data phase. If > 0 then bitrate switching is enabled. Unit: kBit/s

xSupport29Bits

BOOL

FALSE: only 11-Bit IDs, TRUE: support also 29-Bit

szMemSize

CAA.SIZE

size of memory in bytes

pMemory

POINTER TO BYTE

pointer to aligned memory

peError

POINTER TO ERROR

optional pointer to error enum