_Read (FUN)
FUNCTION _Read : CAA.HANDLE
Unmanaged implementation of Read
- InOut:
Scope
Name
Type
Comment
Return
_ReadCAA.HANDLEhandle of received CAN message or
CAA.gc_hINVALIDif receiver is empty.Input
hReceiverIdCAA.HANDLEreceiver handle
pctMsgLeftPOINTER TO CAA.COUNT
Optional pointer to
ctMsgLeft. After callingCL2.ReadctMsgLeftcontains the number of remaining messages in receive queue.peErrorPOINTER TO ERROR
optional pointer to error enum