_CreateMaskReceiver (FUN)
FUNCTION _CreateMaskReceiver : CAA.HANDLE
Unmanaged implementation of CreateMaskReceiver
- InOut:
Scope
Name
Type
Comment
Return
_CreateMaskReceiverCAA.HANDLEnew receiver handle or
CAA.gc_hINVALIDin case of failureInput
hDriverCAA.HANDLEhandle of CAN interface
cobIdValueCL2I.COBIDCobID value
cobIdMaskCL2I.COBIDCobID mask
xRTRValueBOOLRTR value
xRTRMaskBOOLRTR mask
x29BitIdValueBOOL29 Bit Id value
x29BitIdMaskBOOL29 Bit Id mask
xTransmitValueBOOLTransmit message value
xTransmitMaskBOOLTransmit message mask
xAlwaysNewestBOOLTRUE: returns only the newest message; FALSE: receiver with queue.
eEventCB.EVENTtrigger event when message received
xEnableSyncWindowBOOLuse SYNC window: not implemented ==> do not care
peErrorPOINTER TO ERROR
optional pointer to error enum