_DriverOpenH (FUN)
FUNCTION _DriverOpenH : CAA.HANDLE
Unmanaged implementation of DriverOpenH
- InOut:
Scope
Name
Type
Comment
Return
_DriverOpenHCAA.HANDLEhandle of CAN interface or
CAA.gc_hINVALIDif failed.Input
usiNetIdUSINTnumber of CAN network [0..n]
uiBaudrateUINTBaudrate in kBit/s
xSupport29BitsBOOLFALSE: only 11-Bit IDs, TRUE: support also 29-Bit
ctMessagesCAA.COUNTnumber of transmit messages which should be allocated
peErrorPOINTER TO ERROR
optional pointer to error enum