_ReadArrayReceiver (FUN)
FUNCTION _ReadArrayReceiver : CAA.HANDLE
Reads messages from an Array Receiver created by _CreateArrayReceiver
- InOut:
Scope
Name
Type
Comment
Return
_ReadArrayReceiverCAA.HANDLEhandle of received CAN message or
CAA.gc_hINVALIDif receiver is empty.Input
hArrayReceiverCAA.HANDLEhandle of array receiver
ctIndexCAA.COUNTspecifies the array entry which should be read
pctMsgLeftPOINTER TO CAA.COUNT
returns number of messages currently in the receiver
peErrorPOINTER TO ERROR
optional pointer to error enum