_CreateSingleIdReceiver (FUN)
FUNCTION _CreateSingleIdReceiver : CAA.HANDLE
Unmanaged implementation of CreateSingleIdReceiver
- InOut:
Scope
Name
Type
Comment
Return
_CreateSingleIdReceiverCAA.HANDLEnew receiver handle or
CAA.gc_hINVALIDin case of failureInput
hDriverCAA.HANDLEhandle of CAN interface
cobIdCL2I.COBIDid of message to be received
xRTRBOOLRTR bit
x29BitIdBOOL29 Bit Id
xTransmitBOOLTransmit message
xAlwaysNewestBOOLTRUE: returns only the newest message; FALSE: receiver with queue.
eEventCB.EVENTtrigger event when message received
xEnableSyncWindowBOOLuse SYNC window: not implemented ==> do not care
peErrorPOINTER TO ERROR
optional pointer to error enum