_FdDriverOpenH (FUN)

FUNCTION _FdDriverOpenH : CAA.HANDLE

Unmanaged implementation of FdDriverOpenH

InOut:

Scope

Name

Type

Comment

Return

_FdDriverOpenH

CAA.HANDLE

Input

usiNetId

USINT

number of CAN interface [0..n]

uiNominalBaudrate

UINT

Baudrate used for arbitration. Unit: kBit/s

uiDataBaudrate

UINT

Baudrate used for data phase. If > 0 then bitrate switching is enabled. Unit: kBit/s

xSupport29Bits

BOOL

FALSE: only 11-Bit IDs, TRUE: support also 29-Bit

ctMessages

CAA.COUNT

number of FD transmit messages which should be allocated

peError

POINTER TO ERROR

optional pointer to error enum