Library
2.9.0
  • ABB - AC500
  • CODESYS - Application
  • CODESYS - Use Cases
  • CODESYS - System
    • SysLibs
      • CmpApp (LIB)
      • CmpAppBP (LIB)
      • CmpAsyncMgr (LIB)
      • AlarmManagerToOpcUaConnector (LIB)
      • CmpBACnet (LIB)
      • CmpBinTagUtilIec (LIB)
      • CmpBitmapPool (LIB)
      • CmpChannelClientIec (LIB)
      • CmpChecksum (LIB)
      • CmpCodeMeter (LIB)
      • CmpCrypto Implementation (LIB)
      • CmpCrypto (LIB)
      • CmpCrypto Interfaces (LIB)
      • CmpDynamicText (LIB)
      • CmpErrors2 Interfaces (LIB)
      • CmpEventMgr Implementation (LIB)
      • CmpEventMgr (LIB)
      • CmpEventMgr Interfaces (LIB)
      • CmpHilscherCIFX (LIB)
      • CmpIecTask (LIB)
      • CmpIecVarAccess Implementation (LIB)
      • CmpIecVarAccess (LIB)
      • CmpIecVarAccess Interfaces (LIB)
      • CmpIoMgr Implementation (LIB)
      • CmpIoMgr (LIB)
      • CmpIoMgr Interfaces (LIB)
      • CmpKNX (LIB)
      • CmpLog (LIB)
      • CmpLogAsync (LIB)
      • CmpNameServiceClientIec (LIB)
      • CmpOPCUAClient Implementation (LIB)
      • CmpOPCUAClient (LIB)
      • CmpOPCUAClient Interfaces (LIB)
      • CmpOPCUAProviderAlarmConfiguration Implementation (LIB)
      • CmpOPCUAProviderAlarmConfiguration (LIB)
      • CmpOPCUAProviderAlarmConfiguration Interfaces (LIB)
      • CmpOPCUAServer Implementation (LIB)
      • CmpOPCUAServer (LIB)
      • CmpOPCUAServer Interfaces (LIB)
      • CmpOPCUAStack Implementation (LIB)
      • CmpOPCUAStack (LIB)
      • CmpOPCUAStack Interfaces (LIB)
      • CmpRouter (LIB)
      • CmpSchedule (LIB)
      • CmpSettings (LIB)
      • CmpSrv (LIB)
      • CmpTargetVisu (LIB)
      • CmpTls Implementation (LIB)
      • CmpTls (LIB)
      • CmpTls Interfaces (LIB)
      • CmpTraceMgr (LIB)
      • CmpUserMgr Implementation (LIB)
      • CmpUserMgr (LIB)
      • CmpUserMgr Interfaces (LIB)
      • CmpVisuHandler (LIB)
      • CmpWebServer Implementation (LIB)
      • CmpWebServer (LIB)
      • CmpWebServer Interfaces (LIB)
      • CmpX509Cert Implementation (LIB)
      • CmpX509Cert (LIB)
      • CmpX509Cert Interfaces (LIB)
      • Component Manager (LIB)
      • NotImplementedByDevice (LIB)
      • SysCom (LIB)
      • SysComAsync (LIB)
      • SysCpuHandling (LIB)
      • SysCpuMultiCore (LIB)
      • SysDir (LIB)
      • SysEthernet (LIB)
        • Description
        • Contents:
          • SysEthernet
            • Constants
            • EventParameter
            • Functions
              • SysEthernetAdapterClose (FUN)
              • SysEthernetAdapterOpen (FUN)
              • SysEthernetEthFrameReceive (FUN)
              • SysEthernetEthFrameSend (FUN)
              • SysEthernetFrameRelease (FUN)
              • SysEthernetGetCapabilities (FUN)
              • SysEthernetGetInterfaceCounters (FUN)
              • SysEthernetGetMediaCounters (FUN)
              • SysEthernetGetPortConfigAndStatus (FUN)
              • SysEthernetIpFrameReceive (FUN)
              • SysEthernetIpFrameSend (FUN)
              • SysEthernetLEDBlink (FUN)
              • SysEthernetSetAutoNegAdvertisedCap (FUN)
              • SysEthernetSetAutoNegMode (FUN)
              • SysEthernetSetMauType (FUN)
            • Structs
        • Indices and tables
      • SysEvent (LIB)
      • SysExcept (LIB)
      • SysFile (LIB)
      • SysMem (LIB)
      • SysProcess Implementation (LIB)
      • SysProcess (LIB)
      • SysProcess Interfaces (LIB)
      • SysSem Implementation (LIB)
      • SysSem (LIB)
      • SysSem Interfaces (LIB)
      • SysShm Implementation (LIB)
      • SysShm (LIB)
      • SysShm Interfaces (LIB)
      • SysSocket Implementation (LIB)
      • SysSocket (LIB)
      • SysSocket2 Implementation (LIB)
      • SysSocket2 (LIB)
      • SysSocket2 Interfaces (LIB)
      • SysSocketAsync (LIB)
      • SysSocket Interfaces (LIB)
      • SysTarget (LIB)
      • SysTask (LIB)
      • SysTime (LIB)
      • SysTimeCore (LIB)
      • SysTimeRtc (LIB)
      • SysTypes2 Interfaces (LIB)
    • Redundancy
  • CODESYS - Intern
Library
  • »
  • CODESYS - System »
  • SysLibs »
  • SysEthernet (LIB) »
  • SysEthernet »
  • Functions »
  • SysEthernetLEDBlink (FUN)

SysEthernetLEDBlink (FUN)

FUNCTION SysEthernetLEDBlink : SysTypes.RTS_IEC_RESULT

Triggering the mechanism to blink a LED of an adapter specified by the MAC address for the specified duration. The operating system and hardware must support this feature. The function call doesn’t wait the given duration and returns as fast as possible. However the real-time capability of this call is not guranteed.

InOut:

Scope

Name

Type

Comment

Return

SysEthernetLEDBlink

SysTypes.RTS_IEC_RESULT

Runtime system error code (see CmpErrors.library).

Input

macAddress

ARRAY [0..5] OF BYTE

MAC address of the adapter that should blink.

durationInSec

UDINT

Duration to blink the adapter in seconds

Next Previous

© Copyright 2025, ABB.