SysComAsyncFB.SysComCloseAsync (METH)
METHOD SysComCloseAsync : RTS_IEC_HANDLE
<description>Close a com port asynchronously</description> <result><p>RESULT: Returns the runtime system error code (see CmpErrors.library).</p></result>
- InOut:
Scope
Name
Type
Comment
Return
SysComCloseAsyncRTS_IEC_HANDLEInput
pParamPOINTER TO tSysComClose
<param name=”pParam” type=”IN”></param>
pudStatePOINTER TO UDINT
<param name=”pudState” type=”IN”>State of the async job. See CmpAsyncMgr.GVL.ASYNCSTATE_ definitions in CmpAsyncMgr.library.</param>
pResultPOINTER TO RTS_IEC_RESULT
<param name=”pResult” type=”OUT”>Pointer to runtime system error code (see CmpErrors.library)</param>