EventIDs (GVL)
- InOut:
Scope
Name
Type
Initial
Comment
Constant
EVTPARAMID_CmpMgr_Shutdown
WORD16#1
IDs for the event parameter structures
EVTVERSION_CmpMgr_Shutdown
WORD16#1
EVTPARAMID_CmpMgr_DisableOperation
WORD16#2
EVTVERSION_CmpMgr_DisableOperation
WORD16#1
EVTPARAMID_CmpMgr_PrepareExitCommProcessing
WORD16#3
EVTVERSION_CmpMgr_PrepareExitCommProcessing
WORD16#1
EVTPARAMID_CmpMgr_LicenseRequest
WORD16#4
EVTVERSION_CmpMgr_LicenseRequest
WORD16#1
EVTPARAMID_CMPMGR_LICENSE_STATE
WORD16#5
EVTVERSION_CMPMGR_LICENSE_STATE
WORD16#1
EVT_CmpMgr_PrepareShutdown
DWORD16#10001
<category>Events</category> <description>Event is sent right before shutdown of the runtime system</description> <param name=”pEventParam” TYPE=”IN”>EVTPARAM_CmpMgr_Shutdown</param>
EVT_CmpMgr_PrepareExitComm
DWORD16#10002
<category>Events</category> <description>Event is sent before exit the communication servers during shutdown</description> <param name=”pEventParam” TYPE=”IN”>EVTPARAM_CmpMgr_Shutdown</param>
EVT_CmpMgr_PrepareExitTasks
DWORD16#10003
<category>Events</category> <description>Event is sent before exit all tasks during shutdown</description> <param name=”pEventParam” TYPE=”IN”>EVTPARAM_CmpMgr_Shutdown</param>
EVT_CmpMgr_DisableOperation
DWORD16#10006
<category>Events</category> <description>Event is sent TO disable operations. Each operation is defined in the corresponding Itf.h file OF the component, which is specified BY its ComponentID</description> <param name=”pEventParam” TYPE=”IN”>EVTPARAM_CmpMgr_DisableOperation</param>
EVT_CmpMgr_PrepareExitCommProcessing
DWORD16#10007
<category>Events</category> <description>Event is sent after <see>EVT_CmpMgr_PrepareExitComm</see> and can be used if comm cycles are necessary to perform some kind of shutdown operation. The event may be called several times if one of the callees requests further calls. This can happen if the shutdown operation takes some time.</description> <param name=”pEventParam” TYPE=”IN”>EVTPARAM_CmpMgr_Shutdown</param>
EVT_CmpMgr_LicenseRequest
DWORD16#10008
<category>Events</category> <description>Event to get informed when a license was requrested. Only for informational use. No result of the event will be evaulated.</description> <param name=”pEventParam” type=”IN”>EVTPARAM_CmpMgr_LicenseRequest</param>
EVT_CmpMgr_LicenseState
DWORD16#10009
<category>Events</category> <description>Event is sent with each transition of the license statemachine and at certain times before shutdown due to demomode or license lost.</description>
<param name=”pEventParam” type=”IN”>EVTPARAM_CmpMgr_LicenseState</param>