EventIDs (GVL)

Attributes:
qualified_only
InOut:

Scope

Name

Type

Initial

Comment

Constant

CMPID_CmpWebServer

DWORD

16#71

ComponentID to specify for EventOpen

EVT_WebserverFileProtectionQuery

DWORD

(SHL(UINT_TO_DWORD(EventClass.EVTCLASS_INFO), 16) OR 16#1)

Event is sent when the webserver is starting.

If this is event is active, it is possible to activate the file protection with the function WebsFileAccessProtectionActivate.