WebsFileAccessProtectionActivate (FUN)

FUNCTION WebsFileAccessProtectionActivate : RTS_IEC_RESULT

<description>Activates the file protection in the webserver using a whitelist. This function can only be called after there was an runtime event with the Id: EVT_WebserverFileProtectionQuery.</description> <result><p>RESULT: Returns the runtime system error code (see CmpErrors.library).</p></result>

InOut:

Scope

Name

Type

Return

WebsFileAccessProtectionActivate

RTS_IEC_RESULT