EventIDs (GVL)
- Attributes:
qualified_only- InOut:
Scope
Name
Type
Initial
Comment
Constant
CMPID_CmpUserMgr
DWORD16#61
EVTPARAMID_CmpUserMgrDatabaseChanged
WORD16#1
EVTVERSION_CmpUserMgrDatabaseChanged
WORD16#1
EVT_UserMgrDatabaseChanged
DWORD(SHL(UINT_TO_DWORD(EVTCLASS_INFO), 16) OR 16#1)
Event is sent every time the user management database or the user-rights database was changedpEventParam: EVTPARAM_CmpUserMgrDatabaseChangedEVTPARAMID_CmpUserMgrPasswordValidity
WORD16#3
EVTVERSION_CmpUserMgrPasswordValidity
WORD16#1
EVT_UserMgrPasswordValidity
DWORD(SHL(UINT_TO_DWORD(EVTCLASS_INFO), 16) OR 16#5)
Event is fired at PLC start, after an application download and then once a day to inform about password validity with time info. In case a password is expired EVT_UserMgrPasswordExpired is fired instead.pEventParam: EVTPARAM_CmpUserMgrPasswordValidityEVT_UserMgrPasswordExpired
DWORD(SHL(UINT_TO_DWORD(EVTCLASS_WARNING), 16) OR 16#6)
Check is done at PLC start, after an application download and then once a day. An event is fired in case a password is expired due to timeout, instead of EVT_UserMgrPasswordValidity.Event is also fired at login with expired password. The time info is 0 if it is a relogin or a created user is required to change the password on first use.pEventParam: EVTPARAM_CmpUserMgrPasswordValidity