UserMgrUserAdd (FUN)
FUNCTION UserMgrUserAdd : RTS_IEC_RESULT
Add a new user to the user database
- InOut:
Scope
Name
Type
Comment
Return
UserMgrUserAddRTS_IEC_RESULT- Error code
ERR_OK: User could be added
ERR_DUPLICATE: User already exists
ERR_PARAMETER: Invalid parameter. pszUser empty
ERR_NOMEMORY: No memory available to store new user
ERR_NOTINITIALIZED: The user management is not initialized or it is not loaded yet
ERR_NO_ACCESS_RIGHTS: User not authorized
ERR_PASSWORD_POLICY: Password does not fulfill the password policy requirements
Input
hUserRTS_IEC_HANDLEHandle to authorized user
Inout Const
pszUserSTRINGUser name, limited to 59 chars
pCredentialsUserMgrCredentialsCredentials, only password is available so far, password (plain text) is limited to 59 chars