UserMgrHasUserAccessRights (FUN)
FUNCTION UserMgrHasUserAccessRights : RTS_IEC_RESULT
Checks user access rights on the specified object (authorization)!
- InOut:
Scope
Name
Type
Comment
Return
UserMgrHasUserAccessRightsRTS_IEC_RESULT- Error code
ERR_OK: If user has the requested rights on the object or if no user management is configured
ERR_PARAMETER: If user is not available or the object does not exist
ERR_FAILED: If something failed retrieving the access rights
ERR_NO_ACCESS_RIGHTS: Explicitly denied rights
ERR_INVALID_HANDLE: hUser is invalid or unknown
Input
pszObjectREFERENCE TO STRING
Full object name (see object tree)
hUserRTS_IEC_HANDLEHandle to the user
ulRequestedRightsDWORDRequested rights on that object