UserMgrChangeMyPassword (FUN)

FUNCTION UserMgrChangeMyPassword : RTS_IEC_RESULT

Changes the users password

InOut:

Scope

Name

Type

Comment

Return

UserMgrChangeMyPassword

RTS_IEC_RESULT

Error code
  • ERR_OK: Password changed successfully

  • ERR_NOTINITIALIZED: The user management is not initialized or it is not loaded yet

  • ERR_OPERATION_DENIED: Password change is either not supported or not allowed

  • ERR_USER_MISMATCH: User name does not match

  • ERR_INVALID_HANDLE: hUser is invalid or unknown

  • ERR_PASSWORD_POLICY: Password does not fulfill the password policy requirements

Input

hUser

RTS_IEC_HANDLE

Handle to the user

pszUser

REFERENCE TO STRING

Name of the user, limited to 59 chars

pszOldPassword

REFERENCE TO STRING

Old password (plain text), limited to 59 chars

pszNewPassword

REFERENCE TO STRING

New password (plain text), limited to 59 chars