OpcUaServerExternalRedundancySetServers (FUN)

FUNCTION OpcUaServerExternalRedundancySetServers : RTS_IEC_RESULT

Configure the redundant OPC UA Servers, if the OPC UA Redundancy is managed via some external tool. Changes will take effect immediately. Note: The Redundancy.Mode must be configured to External. Note: OpcUaServerSetExternalRedundancyMode must not be set to None.

InOut:

Scope

Name

Type

Comment

Return

OpcUaServerExternalRedundancySetServers

RTS_IEC_RESULT

Result of the operation. ERR_PARAMETER if one of the parameters was invalid. ERR_NOT_SUPPORED if the OPC UA Server is not setup for external redundancy. ERR_OK if Values are recognized by the server.

Input

redundantServers

POINTER TO OpcUa_ApplicationDescription

The ApplicationDescriptions of the redundant OPC UA Servers to show within the address space and FindServers.

numRedundantServers

OpcUa_UInt32

The number of URIs given.