IOPCUAClientMonitoredItemCallback.ItemParameterCallback (METH)

METHOD ItemParameterCallback : OpcUa_StatusCode

The callback is called when the parameters of a monitored item (both event and sampling) has changed. This happens typically after creation (OpcUaClient_CreateMonitoredItem) or modification (OpcUaClient_ModifyMonitoredItems) of a monitored item. The values in this call represent the reviced parameters from the server.

InOut:

Scope

Name

Type

Comment

Return

ItemParameterCallback

OpcUa_StatusCode

Input

hMonitoredItem

RTS_IEC_HANDLE

Handle to the moniotred item.

monitoringMode

OpcUa_MonitoringMode

The new monitoring mode

samplingInterval

OpcUa_Double

The reviced sampling interval for sampling items.

queueSize

OpcUa_UInt32

The reviced queue size.

filter

OpcUa_ExtensionObject

The reviced filters.

reason

OpcUa_StatusCode

Status code if the operation was successful.