EVTPARAM_PacketConfirmation (STRUCT)

TYPE EVTPARAM_PacketConfirmation : STRUCT

InOut:

Name

Type

Comment

hPkt

CAA.Handle

Handle of the confirmation packet

udiPutInQueue

UDINT

Deprecated: Flag, if the packet should be placed in a queue or not. If it is 0, packet is discarded after this callback

udiGenerateAsyncEvent

UDINT

Deprecated: Flag, if a asynchronous event should be generated (only with CAA Callback included)

eAsyncEvent

INT

Deprecated: CB.EVENT - CAA Callback event, which should be posted.