CreateSingleIdReceiver (FUN)
FUNCTION CreateSingleIdReceiver : CAA.HANDLE
This function creates a receiver for one specific CAN identifier. For receiving a message use the returned receiver handle for Read function call. There are two kind of receivers:
Always Newest Receivers (xAlwaysNewest := TRUE): Receiver holds only the last received message.
Receiver with Queue (xAlwaysNewest := FALSE): Receiver holds messages in chronological order.
Receivers can be also used for Tx loopback. If xTransmit is set to TRUE CAN messages which are sent via Write will be received
(applies to all transmit messages on the CAN interface).
Use function IsTransmitMessage to distinguish between receive and transmit messages.
Note
To avoid losing receive messages an application has to read all messages of a receiver each cycle. All messages should be processed and released by FreeMessage afterwards.
Example
In this example a single ID receiver is created. It receives all RTR messages on CAN ID 16#100.
VAR
hDriver : CAA.HANDLE;
hReceiver : CAA.HANDLE;
hMsg : CAA.HANDLE;
pData : POINTER TO CL2I.DATA;
eError : CL2.ERROR;
ctMsgLeft : CAA.COUNT;
END_VAR
hReceiver := CL2.CreateSingleIdReceiver(hDriver := hDriver,
cobId := 16#100,
xRTR := TRUE,
x29BitId := FALSE,
xTransmit := FALSE,
xAlwaysNewest := FALSE,
eEvent := CB.EVENT.NO_EVENT, //no receive event
xEnableSyncWindow := FALSE, //not implemented
peError := ADR(eError) //optional pointer to error
);
REPEAT
//receive a message from hReceiver
hMsg := CL2.Read(hReceiverId := hReceiver, pctMsgLeft := ADR(ctMsgLeft), peError := ADR(eError));
IF hMsg <> CAA.gc_hINVALID THEN
//TODO: Process message (CL2.GetMessageDataPointer, CL2.GetMessageId, ...)
CL2.FreeMessage(hMsg); //release message
hMsg := CAA.gc_hINVALID; //to avoid using an already released message
END_IF
UNTIL ctMsgLeft = 0
END_REPEAT
Optionally, an event can be registered which is triggered upon reception of a corresponding message.
A callback function can be registerd via CB.RegisterCallback (CAA Callback library).
Use event class CB.EVENT_CLASS.FIELDBUS, event source CB.EVENT_SOURCE.CB_DRIVER and any unassigned event number (see CB.EVENT).
Use the same event number for eEvent input.
Input variable dwParam of the registered callback function contains the CAN ID of the received message.
Note
Event mechanism is not supported on all systems. Futhermore it is not possible to register an event for extended identifiers (29bit).
Example
In this example a single ID receiver with event callback is created.
Step 1: Define a callback function with following interface (function name can be changed!).
FUNCTION CallbackReceiveCANMessage : DWORD
VAR_INPUT
dwSpec : DWORD; (* CB.Event and CB.EventClass *)
dwSource : DWORD; (* CB.EventSource *)
dwParam : DWORD; (* CAN ID *)
END_VAR
Step 2: Activate Enable system call in build settings of CallbackReceiveCANMessage.
Step 3: Register callback and create receiver.
VAR
hDriver : CAA.HANDLE;
hReceiver : CAA.HANDLE;
eError : CL2.ERROR;
callback : CB.CB_CALLBACK;
hEvent : CAA.HANDLE;
eCBError : CB.ERROR;
END_VAR
callBack.eClass := CB.EVENT_CLASS.FIELDBUS;
callback.eSource := CB.EVENT_SOURCE.DRIVER;
callback.eEvent := 10000; //any unassigned event number
callback.pPOUFunc := ADR(CallbackReceiveCANMessage);
hEvent := CB.RegisterCallback(callback, ADR(eCBError));
hReceiver := CL2.CreateSingleIdReceiver(hDriver := hDriver,
cobId := 16#100,
xRTR := FALSE,
x29BitId := FALSE,
xTransmit := FALSE,
xAlwaysNewest := FALSE,
eEvent := 10000, //use the previously registered event number
xEnableSyncWindow := FALSE, //not implemented
peError := ADR(eError) //optional pointer to error
);
- InOut:
Scope
Name
Type
Comment
Return
CreateSingleIdReceiverCAA.HANDLEnew receiver handle or
CAA.gc_hINVALIDin case of failureInput
hDriverCAA.HANDLEhandle of CAN interface
cobIdCL2I.COBIDid of message to be received
xRTRBOOLTRUE: receive RTR messages,FALSE: receive no RTR messagesx29BitIdBOOLTRUE: receive 29 Bit Ids,FALSE: receive 11 Bid IdsxTransmitBOOLTRUE: receive Tx messages,FALSE: receive Rx messagesxAlwaysNewestBOOLTRUE: returns only the newest message;FALSE: receiver with queue.eEventCB.EVENTtrigger event when message received
xEnableSyncWindowBOOLuse SYNC window: not implemented ==> do not care
peErrorPOINTER TO ERROR
optional pointer to error enum