FdDriverGetSize (FUN)
FUNCTION FdDriverGetSize : CAA.SIZE
Calculates the required memory size for FdDriverOpenP.
- InOut:
Scope
Name
Type
Comment
Return
FdDriverGetSizeCAA.SIZERequired memory size in bytes for FdDriverOpenP
Input
usiNetIdUSINTnumber of CAN interface [0..n]
xSupport29BitBOOLFALSE: only 11-Bit IDs,TRUE: support also 29-BitctMessagesCAA.COUNTnumber of transmit messages which should be allocated
peErrorPOINTER TO ERROR
optional pointer to error enum