FreeMessage (FUN)
FUNCTION FreeMessage : ERROR
This function releases a message that has been created with CreateMessage, read with Read or duplicated with CloneMessage.
Note
Do not free a message after it has been passed to the CL2 layer.
Example: Creating a message, then passing the message handle to CL2 by calling Write and releasing it afterwards may result in unexpected behaviour.
- InOut:
Scope
Name
Type
Comment
Return
FreeMessageERROR.NO_ERROR or appropriate error code
Input
hMessageCAA.HANDLEhandle of message to be freed