CreateIdAreaReceiver (FUN)
FUNCTION CreateIdAreaReceiver : CAA.HANDLE
This function creates a receiver to which several identifier areas may be added using the function RegisterIdArea. This receiver type is used if messages within a specific cobID area should be received. For receiving a message use the returned receiver handle for Read function call. There are two kind of receivers:
Always Newest Receivers (xAlwaysNewest := TRUE): Receiver holds only the last received message.
Receiver with Queue (xAlwaysNewest := FALSE): Receiver holds messages in chronological order.
Note
To avoid losing receive messages an application has to read all messages of a receiver each cycle. All messages should be processed and released by FreeMessage afterwards.
Note
Current implementation of this receiver type does not support 29 bit identifiers.
Example
VAR
hDriver : CAA.HANDLE;
hReceiver : CAA.HANDLE;
hMsg : CAA.HANDLE;
ctMsgLeft : CAA.COUNT;
eError : CL2.ERROR;
END_VAR
//Create an IdAreaReceiver
hReceiver := CL2.CreateIdAreaReceiver(hDriver := hDriver, //driver handle
xAlwaysNewest := FALSE, //FALSE ==> receiver with queue; TRUE ==> only newest message
eEvent := CB.EVENT.NO_EVENT, //no receive event
xEnableSyncWindow := FALSE, //not implemented
peError := ADR(eError) //optional pointer to error
);
IF hReceiver <> CAA.gc_hINVALID THEN
//Add an area for CANopen Emergency messages (cobId 16#81-16#9F)
CL2.RegisterIdArea(hReceiverId := hReceiver, //receiver
cobIdStart := 16#81, //start cobID
cobIdEnd := 16#9F, //end cobID
xRTRValue := FALSE, //no RTR messages
xRTRMask := TRUE, //activate RTR filter ==> xRTRValue will be checked
x29BitIdValue := FALSE, //no 29 bit CAN messages
x29BitIdMask := TRUE, //activate 29 bit filter ==> x29BitIdValue will be checked
xTransmitValue := FALSE, //only receive messages, no transmit message loopback
xTransmitMask := TRUE //activate transmit mask filter ==> xTransmitValue will be checked
);
END_IF
REPEAT
//receive a message from hReceiver
hMsg := CL2.Read(hReceiverId := hReceiver, pctMsgLeft := ADR(ctMsgLeft), peError := ADR(eError));
IF hMsg <> CAA.gc_hINVALID THEN
//TODO: Process message (CL2.GetMessageDataPointer, CL2.GetMessageId, ...)
CL2.FreeMessage(hMsg); //release message
hMsg := CAA.gc_hINVALID; //to avoid using an already released message
END_IF
UNTIL ctMsgLeft = 0
END_REPEAT
Optionally, an event can be registered which is triggered upon reception of a corresponding message.
A callback function can be registerd via CB.RegisterCallback (CAA Callback library).
Use event class CB.EVENT_CLASS.FIELDBUS, event source CB.EVENT_SOURCE.CB_DRIVER and any unassigned event number (see CB.EVENT).
Use the same event number for eEvent input.
Input variable dwParam of the registered callback function contains the CAN ID of the received message.
See CreateSingleIdReceiver for example code.
Note
Event mechanism is not supported on all systems. Futhermore it is not possible to register an event for extended identifiers (29bit).
- InOut:
Scope
Name
Type
Comment
Return
CreateIdAreaReceiverCAA.HANDLEnew receiver handle or
CAA.gc_hINVALIDin case of failureInput
hDriverCAA.HANDLEhandle of CAN interface
xAlwaysNewestBOOLTRUE: returns only the newest message; FALSE: receiver with queue.
eEventCB.EVENTtrigger event when message received
xEnableSyncWindowBOOLuse SYNC window: not implemented ==> do not care
peErrorPOINTER TO ERROR
optional pointer to error enum